This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5964: ERASE FAILURE IN MSP430FR5964IPNR DEVICE

Part Number: MSP430FR5964


Tool/software:

Hello team,

I am using the MSP430FR5964IPNR device with the DPL language. While attempting to erase data, I’ve encountered an issue where the informative memory is not erasing. It throws an error stating "cannot erase," and I observed that the erase macro in the algorithm fails continuously. However, it works fine with the main memory.

We are using the 80-pin QFP package, and I was able to read the device successfully, but the erase functionality is not working. I have made some changes to align with the specifications but need assistance in resolving this erase issue.

MEMORY MAP ACCORDING TO DATASHEET 

BSL MEMORY [800-8FF]

INFORMATIE MEMORY [C00-CFF]

MAIN MEMORY [2000-21FFF]

brief Explanation how erase works 

step-1 : device reset followed by reset_cmd which it resets the cpu, memory and pheripheral states 

step-2 : jtag communication followed by getdevice_430xv2 function to link the device via Jtag interface 

step-3: power on reset followed by executepor_430xv2 command and ensure the powered in stable state with cpu ready for further operations 

step-4: memory address calculation for address in high and low bits, we are splitting into parts with Jtag interface which high bits holds >> 15 and low bits holds << 1

step-5: EraseFlash_430vx2  which are using sending address to device and initiate the erase process, monitoring the erase status 

step-6: Loop over memory ranges for iterate through blocks for Erase Each page/Block

step-7: Checking Jtag Mailbox flags to verify that erase operation is complete 

step-8: Verification to check memory is erased or not if memory contains all bits cleared(typically set to 0xFF in erased memory)

step-9: Voltage Setting which device operates within specified voltage range during erase process 

step-10: Power On sequence to ensure the device is powered and initialized correctly before erase operation begins.

**Attention** This is a public forum