Part Number: MSP430F5529
Tool/software:
If I am not using the USB functions, do I still need the +5v supply?
I would like to stay at 3.3v.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F5529
Tool/software:
If I am not using the USB functions, do I still need the +5v supply?
I would like to stay at 3.3v.
For the target design. I am using the launchpad now for development but the finished design will not have USB.
But let me ask this:
1) If I include USB, can I program the MSP430 directly from the USB port without the EZ lite chip?
2) Also can I use the two wire programming ports versus full JTAG?
1) Yes you can. You can program the device through USB BSL
2) Yes you can.
**Attention** This is a public forum