Part Number: EVM430-FR6047
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
I just received my EVM430-FR6047 board and followed the User's Guide to set up the device and GUI, but it doesn’t work.
First, I flashed the "MSP430FR6047EVM_USS_Water_Demo_LPM_02_40_00_00.txt" image onto the board using UniFlash 8.8.1. However, when I tried to connect the board through the GUI (USS-02_40_00_00) on my Windows 11, it displayed: "HID device connected, but could not connect to it." I also attempted to connect it in a Ubuntu environment, but the error changed to: "HID Bridge connected -- waiting for device."
I also tried connecting/disconnecting my ultrasound transducer from the board, and nothing changed. Now the LEDs look OK: D101 and D201 are illuminated and D202 blinks.
I have reviewed other related questions on the forum, but none of the solutions resolved the issue.

Does anyone have an idea of how I can fix this issue?
Thank you very much!
Andy