This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2475: Baudrate unstable at low temperatures

Part Number: MSP430FR2475


Tool/software:

Hi 

I have a product, where serial communication fails at low temperatures ( <5 degree celcius ).

I am using the DCO (16MHz) to generate my 115200 Buadrate

I am using an external XTAL at 32768hz.

This is my initialization routine:

const uint16_t u16Ratio = 488U;

/* setup pins for XCLK */
P2SEL0 |= XOUT | XIN;

/* use XCLK as ACLK */
CSCTL6 &= ( uint16_t ) ~ ( ( uint16_t ) DIVA );
CSCTL4 &= ( uint16_t ) ~ ( ( uint16_t ) SELA );

/* set FRAM wait states to 1 */
/*lint -save -e960 */
FRCTL0 = FRCTLPW | NWAITS_1;
/*lint -restore */

/* set ACLK to X Inputs */
CSCTL3 &= ( uint16_t ) ~ ( ( uint16_t ) SELREF_3 );
CSCTL3 |= ( uint16_t ) REFOLP_1;

__bis_SR_register( SCG0 ); /* disable FLL */
/* Set DCO FLL reference = REFO */
CSCTL0 = 0U; /* clear DCO and MOD registers */

CSCTL1 &= ( uint16_t ) ~ ( ( uint16_t ) DCORSEL_7 ); /* Clear DCO frequency select bits first */
CSCTL1 |= ( uint16_t ) DCORSEL_5; /* Set DCO frequency range. DCO Range = 16MHz */
CSCTL2 = ( u16Ratio - 1U ); /* f(DCOCLKDIV) = 16MHz */
CSCTL0 = __data20_read_short( TLV_16MHz_ADDR ); /* load DCO TLV trim vale to DCO Tap */

__delay_cycles( 3U );
__bic_SR_register( SCG0 ); /* enable FLL */

CSCTL4 |= ( uint16_t ) SELMS__REFOCLK; /* set REFO(~32768Hz) as MCLK -- This delay may cause fake lock when DCOTAP=0 */
__delay_cycles( 10U ); /* delay 10 FLL reference clock cycles */

while( ( CSCTL7 & ( ( uint16_t ) FLLUNLOCK0 | ( uint16_t ) FLLUNLOCK1 ) ) > 0U )
{
/* Check if FLL locked */
}
/* set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz */
/* default DCOCLKDIV as MCLK and SMCLK source */
CSCTL4 &= ( uint16_t ) ~ ( ( uint16_t ) SELMS | ( uint16_t ) SELA );

  • Hi Henrik,

    My apologies for the late response. Do you have a way to measure the TXD output bit period both at room temp and at low temperatures?

  • Hi Dennis. 

    I tried to cool the board, but did not see any change on the data line. But I have not seen the problem here. Board works as expected at any temperature.

    I do not yet have any boards of the new production lot, so it may be related to something else.

    But can you confirm my initialization seems correct, and can you confirm that the 2475 should compensate automatically keep the FLL with the external xtal.

  • Hi Henrik,

    You indicated you are using an external 32KHz xtal for the DCO reference, but your code appears to be using the internal REFO, which is also 32KHz, but not as stable as an external xtal across temperatures.

    Here is a copy of MSP430FR2475 clock initialization code that can be found in the TI Resource Explorer.  This should provide stable DCO across temperatures.

        P2SEL0 |= BIT0 | BIT1;                  // P2.0~P2.1: crystal pins
        do
        {
            CSCTL7 &= ~(XT1OFFG | DCOFFG);           // Clear XT1 and DCO fault flag
            SFRIFG1 &= ~OFIFG;
        } while (SFRIFG1 & OFIFG);                   // Test oscillator fault flag
    
        __bis_SR_register(SCG0);                     // disable FLL
        CSCTL3 |= SELREF__XT1CLK;                    // Set XT1 as FLL reference source
        CSCTL1 = DCOFTRIMEN_1 | DCOFTRIM0 | DCOFTRIM1 | DCORSEL_5;// DCOFTRIM=5, DCO Range = 16MHz
        CSCTL2 = FLLD_0 + 487;                       // DCOCLKDIV = 16MHz
        __delay_cycles(3);
        __bic_SR_register(SCG0);                     // enable FLL
        Software_Trim();                             // Software Trim to get the best DCOFTRIM value
    
        CSCTL4 = SELMS__DCOCLKDIV | SELA__XT1CLK;   // set XT1 (~32768Hz) as ACLK source, ACLK = 32768Hz
                                                     // default DCOCLKDIV as MCLK and SMCLK source
    
        P1DIR |= BIT0 | BIT7;                   // set SMCLK ACLK and LED pin as output
        P1SEL1 |= BIT7;                         // set SMCLK P1.7 pin as second function
        P2DIR |= BIT2;
        P2SEL1 |= BIT2;                         // set ACLK P2.2 pin as second function
    
        PM5CTL0 &= ~LOCKLPM5;                        // Disable the GPIO power-on default high-impedance mode
                                                     // to activate previously configured port settings

**Attention** This is a public forum