MSP430FR6047: USS measurement with 8 transducers

Part Number: MSP430FR6047

Tool/software:

Hi,

I hope to use USS measurement with 4pair transducers(8 transducers).

At first I referred to the previous thread here. [USS Measurement with 4 Transducers(2Tx 2Rx)]

And I could download sample source code.

It does well for 4 Transducers(2pair) except the saving parameters(after power off/on all parameters gone).

I confirmed the measurement function on my board with 2 pair transducers.

But I need 4pair, So according to the "SW Specifications Document June 2019" in the package of multi water meter.zip,

I changed the line in USS_userconfig.h, "#define USS_MT_NUM_OF_TRANS_PAIRS    2" => 4. 

But I meet error message when I build project with the code using Code Composer Studio Version: 12.2.0.00009 


"../lnk_msp430fr6047.cmd", line 250: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment fails for section ".data" size 0x174. Available memory ranges:
RAM size: 0x1000 unused: 0x139 max hole: 0x139
error #10010: errors encountered during linking; "MSP430FR6047EVM_USS_Water_Demo.out" not built

How can I solve this error, or is there any new source code for multi pair transducers?

BestRegards

Jack Son

**Attention** This is a public forum