This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Stepper Motor Interfacing -Reg

Hi,

I have one project with stepper motor interface.The motor is 1.8 degree 200 steps/revolution.I want interface motor with Microstepping technique.i don't know how to interface?

Any one please help.

Thanks Inadvance

Regards

Joseph.D

  • Joseph Christober said:
    I have one project with stepper motor interface.The motor is 1.8 degree 200 steps/revolution.I want interface motor with Microstepping technique.i don't know how to interface?

     Hi Joseph, please also specify max motor speed, phase current and voltage or resistance, if you wish to do in software or with a specific chip.

    In case of software the best choice can be in C2000 series but @ low speed also MSP can be used to do pwm modulation of phase sequence.

     Regards

**Attention** This is a public forum