This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2618: MSP430F2618TZCAR power consumption issue

Part Number: MSP430F2618

Tool/software:

Hello,

Problem: Recently, there have been four consecutive cases of high static power consumption after soldering of microcontrollers, with a probability of 1%. The microcontroller model is MSP430F2618TZCAR.

Phenomenon: After PCBA soldering, the static power consumption during testing is relatively high, but the microcontroller functions normally with a normal power consumption of less than 10uA, and the problematic chip has a static power consumption of around 30uA.

The four chips with problems have not undergone rigorous testing such as temperature shock and aging. There are no abnormal power on situations such as high voltage or current.

Please help analyze the reason. Thanks!

**Attention** This is a public forum