Tool/software:
Hi
I currently have 1MHz set up in V configuration. Ands clamped on to a both copper and PEX pipes.
I am using the MSP430FR6047 EVM with the following setup;
Transducers are set at 45 degrees with approximately 5.5cm apart.
Gain is set to -6.5dB but the measurement is receiver side anyway.
Please see attached plots that I am receiving for Copper pipe (CP) and PEX Pipes
CPTIEVM2.pdfPEXTIEVM.pdfPEXTIEVM2.pdfCPTIEVM.pdf
Thanks Calex