This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: Can we drive 8-Com & 12 SEG LCDs , 1/3 bias using MSP430FR6047 as my microcontroller by capacitor split method , instead of internal or external biasing method?

Part Number: MSP430FR6047


Tool/software:

I am observing that the current consumption of 8-Com & 12 SEG LCD , 1/3 bias is 5 microA when i am using capacitor split method of RL-78/L12 series microcontroller. But the current consumption of same LCD is 9.6 microA when i am using internal biasing method of MSP430FR6047. The voltage supply was same in both the cases i.e. 3.6 V. I am assuming that this difference in current consumption is due to these methods only. So, can we implement capacitor split method or not, using MSPFR6047 as my microcontroller. If i can implement this,what should i do?

Is there any other method to drop my LCD current consumption. I have tried to implement external biasing method too , reading from this application note(chrome-extension://efaidnbmnnnibpcajpcglclefindmkaj/www.ti.com/.../slaa654a.pdf)  . But the LCD segments was not behaving properly,showing ghosting effect.The resistor values were R = 100K and Rx(Contrast Control) = 4.7K. It was also showing the ghosting effect. When i was increasing the values of resistors , the ghosting effect was also increasing.

Waiting for a fruitful response.

Thank You

Rishabh Mishra

**Attention** This is a public forum