Hi,
I've recently got hold of an MSP430F5438 Experimenter Board. I set everything up as per the included instructions (installing drivers, ccs, etc..) However, I'm having trouble with the User Experience Demo.
I'm currently running CCS 5.1.0.08020 on an MSP430F5438A microcontroller under Windows XP.
Basically, this is what I did:
1. Run CCS and goto Project --> Import Existing CCS/CCE Eclipse Project
2. Selected the archive file option and browsed to the zip file that contains the user experience demo (slac227j.zip)
3. There are three projects to choose from, I selected MSP-EXP430F5438_User_Experience (the non code-limited one as I'm running a fully functional trial of CCS)
4. Clicked Finish
5. Went to Run --> Debug
And nothing happens. The output I get on the console is:
MSP430: Program loaded. Code Size - Text: 1686 bytes Data: 1162 bytes
MSP430: AutoRun: Target not run as the symbol "main" is not defined
BTW, I tried the Blink LED code example and that works fine.
Any help would be appreciated.
Best Regards,
Husam Ibrahim