Part Number: MSP430FR2311
Tool/software:
Dear Sirs!
I use msp430fr2311 powered from +3.3V, Clock 8MHz from internal generator and PLL without external crystal.
Now I want to start it from +2.0V and after that power it from +1.9V to meet table 5-1 requirements in datasheet.
My question: Can I still clock it 8Mhz as mentioned above or I have to reduce clock?
And additional question:
This device works in narrow temperature range +15C - +40C.
Can I be sure that in this narrow range msp430fr2311 will start from 1.9V? Typical in table 5-1 is 1.88V? What is a minimum voltage that I need to start device in temperature range +15C - +40C?
Please advice
Best regards
Michael