Part Number: MSP430F249
Tool/software:
Hello all I'm attempting to install Code Composer Studio v20.0.1 but am unsuccessful in doing so. I'm on Windows 10 in a corporate environment and am unable to disable endpoint security. I am able to elevate and perform the install as an administrator though by right-clicking on the ccs_setup_20.0.1.00004.exe and doing "run as administrator" but it still errors out. I attempted to also install the 12.8.1.00005.exe Web installer version of CCS but the same issue exists. It seems like it gets to the ti_emu_pack_etc.. and fails. Attached are the install logs. and error report that are generated when the install fails. Additionally I'm using a proxy with authentication so maybe that's also one of the reasons? Also I see in the log the failures with certutil.exe asking for administrator permissions but like I mentioned the installer is running as an administrator. Is there a way to run this from a command prompt?
Log started 01/13/2025 at 10:17:19 Preferred installation mode : win32 Trying to init installer in mode win32 Mode win32 successfully initialized [10:17:23] CCS_INFO: Installer timestamp 20250113101722 [10:17:23] Installer arguments [10:17:23] CCS_INFO: Initialization sets components_download_url to http://software-dl.ti.com/ccs/esd/CCSv20/CCS20.0.1.00004_win64/components Could not find registry key HKEY_LOCAL_MACHINE\SOFTWARE\Texas Instruments\CCS 20.0.1.00004 Version. Setting variable oldVersion to empty value [10:17:23] createshortcuts set to true [10:17:24] CCS_INFO: Temporary folder set to C:\Users\JOEUSER\AppData\Local\Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849 [10:17:25] CCS_INFO: Components available: ARM_MPU_FEATURE_METADATA,AUTO_FEATURE_METADATA,BLACKHAWK_EMUPACK,C2000_FEATURE_METADATA,C29_FEATURE_METADATA,CCS_DOC,CCS_UTILS,CGT_DEFAULTLIBS_C2800,CGT_DEFAULTLIBS_C29,CGT_DEFAULTLIBS_C6000_V8P,CGT_DEFAULTLIBS_MSP430,CLOUDAGENT,DEV_SUPPORT_CC26XX,DEV_SUPPORT_CC3220,DEV_SUPPORT_CC3230,DEV_SUPPORT_CC32XX,DEV_SUPPORT_CC32XX_COMMON,DS,DS_FLASH,ECLIPSE,EMU_C2000_FLASH,EMU_TI,IDE_METADATA,LPCS_FEATURE_METADATA,MMWAVE_FEATURE_METADATA,MSP430_HEADER,MSP430_HEADER_GCC,MSP430_SUPPORT,MSP432_BUILD_DEBUG,MSPM0_FEATURE_METADATA,MSVC_REDIST_LATEST,NODEJS,PF_ARM_MPU,PF_AUTO,PF_C28,PF_C29,PF_C6000SC,PF_HERCULES,PF_MMWAVE,PF_MSP430,PF_MSP432,PF_MSPM0,PF_OMAPL,PF_SITARA_MCU,PF_SP_MCU,PF_TM4C,PF_TM4E,SEGGER_J_LINK,SEGGER_J_LINK_DRIVERS,SHARED_DEVICE_SUPPORT,SITARA_MCU_FEATURE_METADATA,SP_MCU_FEATURE_METADATA,SYSCONFIG,TARGETDB_DEF_PROPS,TARGET_METADATA,THEIA,TIREX,TIVA_STELLARIS_DRIVERS,TI_ARM_CLANG,YAROV [10:17:25] CCS_INFO: Components default folder is set to C:\Users\JOEUSER\Downloads\CCS_20.0.1.00004_win\CCS_20.0.1.00004_win/components [10:17:25] CCS_INFO: Components override folder is set to C:\Users\JOEUSER\Downloads\CCS_20.0.1.00004_win\CCS_20.0.1.00004_win/components [10:17:30] CCS_INFO: Anti-virus detected [10:18:36] CCS_INFO: Testing c:/program files/ in install path c:/ti/ccs2001 [10:18:36] CCS_INFO: Testing c:/program files \(x86\)/ in install path c:/ti/ccs2001 [10:18:36] CCS_INFO: Testing c:/program files/ in install path c:/ti/ccs2001 [10:18:36] Logdir = C:\ti\ccs2001/ccs/install_logs/20250113101722 [10:18:36] CCS_INFO: CCStudio set to C:/ti/ccs2001/ccs/theia/ccstudio.exe [10:18:36] CCS_INFO: setting project.component(CCS_UTILS).selected to 0 [10:18:37] CCS_INFO: setting project.component(TIREX).selected to 0 [10:18:37] CCS_INFO: setting project.component(THEIA).selected to 0 [10:18:37] CCS_INFO: setting project.component(ECLIPSE).selected to 0 [10:18:37] CCS_INFO: setting project.component(NODEJS).selected to 0 [10:18:37] CCS_INFO: setting project.component(DS).selected to 0 [10:18:37] CCS_INFO: setting project.component(DS_FLASH).selected to 0 [10:18:37] CCS_INFO: setting project.component(CLOUDAGENT).selected to 0 [10:18:37] CCS_INFO: setting project.component(SYSCONFIG).selected to 0 [10:18:37] CCS_INFO: setting project.component(EMU_TI).selected to 0 [10:18:37] CCS_INFO: setting project.component(TI_ARM_CLANG).selected to 0 [10:18:37] CCS_INFO: setting project.component(CCS_DOC).selected to 0 [10:18:37] CCS_INFO: setting project.component(TARGETDB_DEF_PROPS).selected to 0 [10:18:37] CCS_INFO: setting project.component(YAROV).selected to 0 [10:18:37] CCS_INFO: setting project.component(TARGET_METADATA).selected to 0 [10:18:37] CCS_INFO: setting project.component(IDE_METADATA).selected to 0 [10:18:37] CCS_INFO: setting project.component(SEGGER_J_LINK).selected to 0 [10:18:37] CCS_INFO: setting project.component(CGT_DEFAULTLIBS_MSP430).selected to 0 [10:18:37] CCS_INFO: setting project.component(CGT_DEFAULTLIBS_C2800).selected to 0 [10:18:37] CCS_INFO: setting project.component(CGT_DEFAULTLIBS_C6000_V8P).selected to 0 [10:18:37] CCS_INFO: setting project.component(CGT_DEFAULTLIBS_C29).selected to 0 [10:18:37] CCS_INFO: setting project.component(TIVA_STELLARIS_DRIVERS).selected to 0 [10:18:37] THEIA NOTSET 20.0.0.20241129081620 [10:18:37] THEIA selected: 1 [10:18:37] THEIA: Installed Version: NOTSET Current Version: 20.0.0.20241129081620 [10:18:37] ECLIPSE NOTSET 20.0.0.202411291303 [10:18:37] ECLIPSE selected: 1 [10:18:37] ECLIPSE: Installed Version: NOTSET Current Version: 20.0.0.202411291303 [10:18:37] DS NOTSET 20.0.0.3612 [10:18:37] DS selected: 1 [10:18:37] DS: Installed Version: NOTSET Current Version: 20.0.0.3612 [10:18:37] DS_FLASH NOTSET 20.0.0.3612 [10:18:37] DS_FLASH selected: 1 [10:18:37] DS_FLASH: Installed Version: NOTSET Current Version: 20.0.0.3612 [10:18:37] CLOUDAGENT NOTSET 0.5.5046 [10:18:37] CLOUDAGENT selected: 1 [10:18:37] CLOUDAGENT: Installed Version: NOTSET Current Version: 0.5.5046 [10:18:37] EMU_TI NOTSET 20.0.0.3283 [10:18:37] EMU_TI selected: 1 [10:18:37] EMU_TI: Installed Version: NOTSET Current Version: 20.0.0.3283 [10:18:37] NODEJS NOTSET 18.16.0 [10:18:37] NODEJS selected: 1 [10:18:37] NODEJS: Installed Version: NOTSET Current Version: 18.16.0 [10:18:37] CCS_UTILS NOTSET 1.0.0.20230823 [10:18:37] CCS_UTILS selected: 1 [10:18:37] CCS_UTILS: Installed Version: NOTSET Current Version: 1.0.0.20230823 [10:18:37] SYSCONFIG NOTSET 1.22.0.3893 [10:18:37] SYSCONFIG selected: 1 [10:18:37] SYSCONFIG: Installed Version: NOTSET Current Version: 1.22.0.3893 [10:18:37] YAROV NOTSET 2.0.1 [10:18:37] YAROV selected: 1 [10:18:37] YAROV: Installed Version: NOTSET Current Version: 2.0.1 [10:18:37] TARGETDB_DEF_PROPS NOTSET 12.3.0.N202303010900 [10:18:37] TARGETDB_DEF_PROPS selected: 1 [10:18:37] TARGETDB_DEF_PROPS: Installed Version: NOTSET Current Version: 12.3.0.N202303010900 [10:18:37] TIREX NOTSET 4.20.0.202411191616 [10:18:37] TIREX selected: 1 [10:18:37] TIREX: Installed Version: NOTSET Current Version: 4.20.0.202411191616 [10:18:37] TI_ARM_CLANG NOTSET 4.0.1.LTS [10:18:37] TI_ARM_CLANG selected: 1 [10:18:37] TI_ARM_CLANG: Installed Version: NOTSET Current Version: 4.0.1.LTS [10:18:37] CCS_DOC NOTSET 20.0.1.00004 [10:18:37] CCS_DOC selected: 1 [10:18:37] CCS_DOC: Installed Version: NOTSET Current Version: 20.0.1.00004 [10:18:37] TARGET_METADATA NOTSET 1.5.2.0 [10:18:37] TARGET_METADATA selected: 1 [10:18:37] TARGET_METADATA: Installed Version: NOTSET Current Version: 1.5.2.0 [10:18:38] IDE_METADATA NOTSET 1.6.1 [10:18:38] IDE_METADATA selected: 1 [10:18:38] IDE_METADATA: Installed Version: NOTSET Current Version: 1.6.1 [10:18:38] SEGGER_J_LINK NOTSET 7.96.0 [10:18:38] SEGGER_J_LINK selected: 1 [10:18:38] SEGGER_J_LINK: Installed Version: NOTSET Current Version: 7.96.0 [10:18:38] CGT_DEFAULTLIBS_MSP430 NOTSET 21.6.1.LTS [10:18:38] CGT_DEFAULTLIBS_MSP430 selected: 1 [10:18:38] CGT_DEFAULTLIBS_MSP430: Installed Version: NOTSET Current Version: 21.6.1.LTS [10:18:38] CGT_DEFAULTLIBS_C2800 NOTSET 22.6.1.LTS [10:18:38] CGT_DEFAULTLIBS_C2800 selected: 1 [10:18:38] CGT_DEFAULTLIBS_C2800: Installed Version: NOTSET Current Version: 22.6.1.LTS [10:18:38] CGT_DEFAULTLIBS_C6000_V8P NOTSET 8.3.13 [10:18:38] CGT_DEFAULTLIBS_C6000_V8P selected: 1 [10:18:38] CGT_DEFAULTLIBS_C6000_V8P: Installed Version: NOTSET Current Version: 8.3.13 [10:18:38] CGT_DEFAULTLIBS_C29 NOTSET 1.0.0.LTS [10:18:38] CGT_DEFAULTLIBS_C29 selected: 1 [10:18:38] CGT_DEFAULTLIBS_C29: Installed Version: NOTSET Current Version: 1.0.0.LTS [10:18:38] TIVA_STELLARIS_DRIVERS NOTSET 2.1.3.15 [10:18:38] TIVA_STELLARIS_DRIVERS selected: 1 [10:18:38] TIVA_STELLARIS_DRIVERS: Installed Version: NOTSET Current Version: 2.1.3.15 [10:18:38] PF_MSPM0 selected: 1 [10:18:38] PF_MSPM0: Installed Version: NOTSET Current Version: 1.12.00.02 [10:18:38] PF_MSP430 selected: 1 [10:18:38] PF_MSP430: Installed Version: NOTSET Current Version: 11.1.0.20211104 [10:18:38] PF_C28 selected: 1 [10:18:38] PF_C28: Installed Version: NOTSET Current Version: 6.23.2.0 [10:18:38] PF_WCONN selected: 1 [10:18:38] PF_ARM_MPU selected: 1 [10:18:38] PF_ARM_MPU: Installed Version: NOTSET Current Version: 1.6.7 [10:18:38] PF_SITARA_MCU selected: 1 [10:18:38] PF_SITARA_MCU: Installed Version: NOTSET Current Version: 1.3.10 [10:18:38] PF_MMWAVE selected: 1 [10:18:38] PF_MMWAVE: Installed Version: NOTSET Current Version: 1.7.17 [10:18:38] PF_HERCULES selected: 1 [10:18:38] PF_HERCULES: Installed Version: NOTSET Current Version: 6.0.9 [10:18:38] PF_TM4C selected: 1 [10:18:39] PF_TM4C: Installed Version: NOTSET Current Version: 2.1.1.15071 [10:18:39] PF_C6000SC selected: 1 [10:18:39] PF_C6000SC: Installed Version: NOTSET Current Version: 1.1.7 [10:18:39] PF_OMAPL selected: 1 [10:18:39] PF_OMAPL: Installed Version: NOTSET Current Version: 1.1.2 [10:18:39] PF_MSP432 selected: 1 [10:18:39] PF_MSP432: Installed Version: NOTSET Current Version: 8.2.2.0 [10:18:39] MSVC_REDIST_LATEST NOTSET 14.38.33135 [10:18:39] MSVC_REDIST_LATEST selected: 1} [10:18:39] SEGGER_J_LINK_DRIVERS NOTSET 1.0.1.0 [10:18:39] SEGGER_J_LINK_DRIVERS selected: 1} [10:18:39] BLACKHAWK_EMUPACK NOTSET 9.0.0.002 [10:18:39] BLACKHAWK_EMUPACK selected: 1} Preparing to Install [10:19:00] CCS_INFO: Components default url is set to http://software-dl.ti.com/ccs/esd/CCSv20/CCS20.0.1.00004_win64/components [10:19:00] CCS_INFO: Components download url is set to http://software-dl.ti.com/ccs/esd/CCSv20/CCS20.0.1.00004_win64/components [10:19:00] CCS_INFO: Starting installation [10:19:00] Install Version : 20.0.1.00004 [10:19:00] Install Source : C:/Users/JOEUSER/Downloads/CCS_20.0.1.00004_win/CCS_20.0.1.00004_win [10:19:00] Install Temp : C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849 [10:19:00] Install Type : Offline [10:19:00] OS : Windows NT [10:19:00] OS Name : Windows 10 [10:19:00] OS Version : 10.0 sp 0 [10:19:00] OS Platform : windows-x64 64-bit [10:19:00] OSD : Windows10-64-bit [10:19:00] User ID : JOEUSER [10:19:00] Timezone : -0800 [10:19:00] InstallTime(GMT): 01/13/2025 18:17:23(GMT) [10:19:00] IPAddress : 10.6.25.87 [10:19:00] Update/Rerun : false [10:19:00] Install GUID : 189a48fc-0982-4df7-5474-cdea126308d4 [10:19:01] Command line : Setting variable proxyInfoTmp from C:\Users\JOEUSER\AppData\Local\Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/util/lsproxy.exe http://www.google.com Script exit code: 0 Script output: proxy-name.domain.com:8080 Script stderr: [10:19:01] CCS_INFO: Running ccs_monitor 20640 C:\Users\JOEUSER\AppData\Local\Temp/mon_1398cd2c-b68f-4b40-7b00-eebb90963849 http://software-dl.ti.com/ccs/esd/tia -x proxy-name.domain.com:8080 Executing C:\Users\JOEUSER\AppData\Local\Temp/mon_1398cd2c-b68f-4b40-7b00-eebb90963849/util/ccs_monitor.bat 20640 "C:\Users\JOEUSER\AppData\Local\Temp/mon_1398cd2c-b68f-4b40-7b00-eebb90963849" http://software-dl.ti.com/ccs/esd/tia/CCS20.0.1.00004_windows-x64_ "-x proxy-name.domain.com:8080" & Script exit code: 0 Script output: Script stderr: [10:19:03] CCS_INFO: Downloading http://software-dl.ti.com/ccs/esd/tia/CCS20.0.1.00004_tia_windows-x64_start_offline.zip [10:19:05] CCS_INFO: Return values from downloadMarker http://software-dl.ti.com/ccs/esd/tia/CCS20.0.1.00004_tia_windows-x64_start_offline.zip: [10:19:05] CCS_INFO: Running install-certs.bat to pre-install driver certificates. Executing C:\Users\JOEUSER\AppData\Local\Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/util/certificates/install-certs.bat Script exit code: unknown signal Script output: C:\Users\JOEUSER\AppData\Local\Temp\ccs_1398cd2c-b68f-4b40-7b00-eebb90963849\util\certificates>C:\WINDOWS\system32\certutil.exe -addstore "TrustedPublisher" C:\Users\JOEUSER\AppData\Local\Temp\CCS_13~1\util\CERTIF~1\\ewa1.p7b Administrator permissions are needed to use the selected options. Use an administrator command prompt to complete these tasks. CertUtil: The requested operation requires elevation. C:\Users\JOEUSER\AppData\Local\Temp\ccs_1398cd2c-b68f-4b40-7b00-eebb90963849\util\certificates>C:\WINDOWS\system32\certutil.exe -addstore "TrustedPublisher" C:\Users\JOEUSER\AppData\Local\Temp\CCS_13~1\util\CERTIF~1\\ewa2.p7b Administrator permissions are needed to use the selected options. Use an administrator command prompt to complete these tasks. CertUtil: The requested operation requires elevation. C:\Users\JOEUSER\AppData\Local\Temp\ccs_1398cd2c-b68f-4b40-7b00-eebb90963849\util\certificates>C:\WINDOWS\system32\certutil.exe -addstore "TrustedPublisher" C:\Users\JOEUSER\AppData\Local\Temp\CCS_13~1\util\CERTIF~1\\ewa3.p7b Administrator permissions are needed to use the selected options. Use an administrator command prompt to complete these tasks. CertUtil: The requested operation requires elevation. C:\Users\JOEUSER\AppData\Local\Temp\ccs_1398cd2c-b68f-4b40-7b00-eebb90963849\util\certificates>C:\WINDOWS\system32\certutil.exe -addstore "TrustedPublisher" C:\Users\JOEUSER\AppData\Local\Temp\CCS_13~1\util\CERTIF~1\\ewa4.p7b Administrator permissions are needed to use the selected options. Use an administrator command prompt to complete these tasks. CertUtil: The requested operation requires elevation. C:\Users\JOEUSER\AppData\Local\Temp\ccs_1398cd2c-b68f-4b40-7b00-eebb90963849\util\certificates>C:\WINDOWS\system32\certutil.exe -addstore "TrustedPublisher" C:\Users\JOEUSER\AppData\Local\Temp\CCS_13~1\util\CERTIF~1\\sd1.p7b Administrator permissions are needed to use the selected options. Use an administrator command prompt to complete these tasks. CertUtil: The requested operation requires elevation. C:\Users\JOEUSER\AppData\Local\Temp\ccs_1398cd2c-b68f-4b40-7b00-eebb90963849\util\certificates>C:\WINDOWS\system32\certutil.exe -addstore "TrustedPublisher" C:\Users\JOEUSER\AppData\Local\Temp\CCS_13~1\util\CERTIF~1\\ti1.p7b Administrator permissions are needed to use the selected options. Use an administrator command prompt to complete these tasks. CertUtil: The requested operation requires elevation. C:\Users\JOEUSER\AppData\Local\Temp\ccs_1398cd2c-b68f-4b40-7b00-eebb90963849\util\certificates>C:\WINDOWS\system32\certutil.exe -addstore "TrustedPublisher" C:\Users\JOEUSER\AppData\Local\Temp\CCS_13~1\util\CERTIF~1\\ti2.p7b Administrator permissions are needed to use the selected options. Use an administrator command prompt to complete these tasks. CertUtil: The requested operation requires elevation. C:\Users\JOEUSER\AppData\Local\Temp\ccs_1398cd2c-b68f-4b40-7b00-eebb90963849\util\certificates>C:\WINDOWS\system32\certutil.exe -addstore "TrustedPublisher" C:\Users\JOEUSER\AppData\Local\Temp\CCS_13~1\util\CERTIF~1\\ti3.p7b Administrator permissions are needed to use the selected options. Use an administrator command prompt to complete these tasks. CertUtil: The requested operation requires elevation. C:\Users\JOEUSER\AppData\Local\Temp\ccs_1398cd2c-b68f-4b40-7b00-eebb90963849\util\certificates>C:\WINDOWS\system32\certutil.exe -addstore "TrustedPublisher" C:\Users\JOEUSER\AppData\Local\Temp\CCS_13~1\util\CERTIF~1\\ti4.p7b Administrator permissions are needed to use the selected options. Use an administrator command prompt to complete these tasks. CertUtil: The requested operation requires elevation. C:\Users\JOEUSER\AppData\Local\Temp\ccs_1398cd2c-b68f-4b40-7b00-eebb90963849\util\certificates>C:\WINDOWS\system32\certutil.exe -addstore "TrustedPublisher" C:\Users\JOEUSER\AppData\Local\Temp\CCS_13~1\util\CERTIF~1\\msp_704.p7b Administrator permissions are needed to use the selected options. Use an administrator command prompt to complete these tasks. CertUtil: The requested operation requires elevation. Script stderr: child killed: unknown signal Error running C:\Users\JOEUSER\AppData\Local\Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/util/certificates/install-certs.bat : child killed: unknown signal [10:19:06] CCS_WARNING: Unable to run install-certs.bat: Error running C:\Users\JOEUSER\AppData\Local\Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/util/certificates/install-certs.bat : child killed: unknown signal: unknown signal [10:19:06] CCS_INFO: Components: [10:19:06] CCS_INFO: BLACKHAWK_EMUPACK: 1 [10:19:06] CCS_INFO: CCS_DOC: 1 [10:19:06] CCS_INFO: CCS_UTILS: 1 [10:19:06] CCS_INFO: CGT_DEFAULTLIBS_C2800: 1 [10:19:06] CCS_INFO: CGT_DEFAULTLIBS_C29: 1 [10:19:06] CCS_INFO: CGT_DEFAULTLIBS_C6000_V8P: 1 [10:19:06] CCS_INFO: CGT_DEFAULTLIBS_MSP430: 1 [10:19:06] CCS_INFO: CLOUDAGENT: 1 [10:19:06] CCS_INFO: DS: 1 [10:19:06] CCS_INFO: DS_FLASH: 1 [10:19:06] CCS_INFO: ECLIPSE: 1 [10:19:06] CCS_INFO: EMU_TI: 1 [10:19:06] CCS_INFO: IDE_METADATA: 1 [10:19:06] CCS_INFO: MSVC_REDIST_LATEST: 1 [10:19:06] CCS_INFO: NODEJS: 1 [10:19:06] CCS_INFO: PF_ARM_MPU: 0 [10:19:06] CCS_INFO: PF_AUTO: 1 [10:19:06] CCS_INFO: PF_C28: 0 [10:19:06] CCS_INFO: PF_C6000SC: 0 [10:19:06] CCS_INFO: PF_HERCULES: 0 [10:19:06] CCS_INFO: PF_MMWAVE: 0 [10:19:06] CCS_INFO: PF_MSP430: 1 [10:19:06] CCS_INFO: PF_MSP432: 0 [10:19:06] CCS_INFO: PF_MSPM0: 0 [10:19:06] CCS_INFO: PF_OMAPL: 0 [10:19:06] CCS_INFO: PF_SITARA_MCU: 0 [10:19:06] CCS_INFO: PF_TM4C: 0 [10:19:06] CCS_INFO: SEGGER_J_LINK: 1 [10:19:06] CCS_INFO: SEGGER_J_LINK_DRIVERS: 1 [10:19:06] CCS_INFO: SYSCONFIG: 1 [10:19:06] CCS_INFO: TARGETDB_DEF_PROPS: 1 [10:19:06] CCS_INFO: TARGET_METADATA: 1 [10:19:06] CCS_INFO: THEIA: 1 [10:19:06] CCS_INFO: TIREX: 1 [10:19:06] CCS_INFO: TIVA_STELLARIS_DRIVERS: 1 [10:19:06] CCS_INFO: TI_ARM_CLANG: 1 [10:19:06] CCS_INFO: YAROV: 1 [10:19:06] CCS_INFO: rerun/update: false Preparing to Install Unpacking files [10:19:13] CCS_INFO: Done installing THEIA Unpacking files [10:19:17] CCS_INFO: Done installing Eclipse Unpacking files [10:19:18] CCS_INFO: Installing DS [10:19:18] showprogress = false [10:19:18] CCS_INFO: Installing C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/DS/ti_dspack_ibsetup_x64_20.0.0.3612.exe [10:19:18] CCS_INFO: Actual executable C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/DS/ti_dspack_ibsetup_x64_20.0.0.3612.exe Executing C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/DS/ti_dspack_ibsetup_x64_20.0.0.3612.exe --prefix "C:\ti\ccs2001/ccs" --eclipseprefix "C:/ti/ccs2001/ccs/eclipse" --mode unattended --installer-log "C:\ti\ccs2001/ccs/install_logs/20250113101722" Script exit code: 0 Script output: Script stderr: [10:19:27] CCS_INFO: Done installing executable DS C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/DS/ti_dspack_ibsetup_x64_20.0.0.3612.exe Unpacking files [10:19:28] CCS_INFO: Done installing DS_FLASH Unpacking files [10:20:17] CCS_INFO: Done installing CLOUDAGENT Unpacking files [10:20:18] CCS_INFO: Installing EMU_TI [10:20:18] showprogress = false [10:20:18] CCS_INFO: Installing C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe [10:20:18] CCS_INFO: Actual executable C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe Executing C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe --prefix "C:\ti\ccs2001/ccs" --eclipseprefix "C:/ti/ccs2001/ccs/eclipse" --mode unattended --installer-log "C:\ti\ccs2001/ccs/install_logs/20250113101722" --enable-components c2800,arm,xds100,xds2xx,xds560,c6000 --disable-components c5500,omap,davinci,scripting,doc Script exit code: Script output: Script stderr: Unknown error while running C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe --prefix "C:\ti\ccs2001/ccs" --eclipseprefix "C:/ti/ccs2001/ccs/eclipse" --mode unattended --installer-log "C:\ti\ccs2001/ccs/install_logs/20250113101722" --enable-components c2800,arm,xds100,xds2xx,xds560,c6000 --disable-components c5500,omap,davinci,scripting,doc [10:21:08] CCS_INFO: Installing C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe [10:21:08] CCS_INFO: Actual executable C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe Executing C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe --prefix "C:\ti\ccs2001/ccs" --eclipseprefix "C:/ti/ccs2001/ccs/eclipse" --mode unattended --installer-log "C:\ti\ccs2001/ccs/install_logs/20250113101722" --enable-components c2800,arm,xds100,xds2xx,xds560,c6000 --disable-components c5500,omap,davinci,scripting,doc Script exit code: Script output: Script stderr: Unknown error while running C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe --prefix "C:\ti\ccs2001/ccs" --eclipseprefix "C:/ti/ccs2001/ccs/eclipse" --mode unattended --installer-log "C:\ti\ccs2001/ccs/install_logs/20250113101722" --enable-components c2800,arm,xds100,xds2xx,xds560,c6000 --disable-components c5500,omap,davinci,scripting,doc [10:21:09] CCS_INFO: Installing C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe [10:21:09] CCS_INFO: Actual executable C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe Executing C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe --prefix "C:\ti\ccs2001/ccs" --eclipseprefix "C:/ti/ccs2001/ccs/eclipse" --mode unattended --installer-log "C:\ti\ccs2001/ccs/install_logs/20250113101722" --enable-components c2800,arm,xds100,xds2xx,xds560,c6000 --disable-components c5500,omap,davinci,scripting,doc Script exit code: Script output: Script stderr: Unknown error while running C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe --prefix "C:\ti\ccs2001/ccs" --eclipseprefix "C:/ti/ccs2001/ccs/eclipse" --mode unattended --installer-log "C:\ti\ccs2001/ccs/install_logs/20250113101722" --enable-components c2800,arm,xds100,xds2xx,xds560,c6000 --disable-components c5500,omap,davinci,scripting,doc [10:21:10] CCS_ERROR: Unable to install executable C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe: Unknown error while running C:/Users/JOEUSER/AppData/Local/Temp/ccs_1398cd2c-b68f-4b40-7b00-eebb90963849/EMU_TI/ti_emupack_setup_20.0.0.3283_win_64.exe --prefix "C:\ti\ccs2001/ccs" --eclipseprefix "C:/ti/ccs2001/ccs/eclipse" --mode unattended --installer-log "C:\ti\ccs2001/ccs/install_logs/20250113101722" --enable-components c2800,arm,xds100,xds2xx,xds560,c6000 --disable-components c5500,omap,davinci,scripting,doc: [10:21:10] CCS_INFO: In installationAbortedActionList [10:21:13] CCS_ERROR: CCS 20.0.1.00004 failed to install. [10:21:13] CCS_INFO: Downloading http://software-dl.ti.com/ccs/esd/tia/CCS20.0.1.00004_tia_windows-x64_failed_offline.zip [10:21:15] CCS_INFO: Return values from downloadMarker http://software-dl.ti.com/ccs/esd/tia/CCS20.0.1.00004_tia_windows-x64_failed_offline.zip: [10:21:15] CCS_INFO: Deleting C:\ti\ccs2001/ccs? : !false [10:21:19] Moving logfile to C:\ti\ccs2001/ccs/install_logs/20250113101722/ccs_install_20.0.1.00004.log
av={Trellix Endpoint Security} {Windows Defender}
logdir=C:\ti\ccs2001/ccs/install_logs/20250109172107
GUID=189a48fc-0982-4df7-5474-cdea126308d4
type=IB
email=joe.user@domain.com