Part Number: MSP430F5308
Other Parts Discussed in Thread: UNIFLASH, MSP-FET
Tool/software:
Hello,
I'm working with an embedded system that contains an MSP430F5308 as a subprocessor gathering sensor data. I've needed to create a homemade cable to connect the MSP-FET to this processor via a JTAG (custom) 10-pin header. For some time, this has worked well, and I have been able to connect/program and erase the processor as needed with UniFlash. Recently I've seen two cases where the UniFlash program cannot connect to the processor at all. The response I get from the software is "No debug probes/devices detected." My workstation is using Windows 11, and the Device Manager reports that the MSP Application UART1 and MSP Debug Interface virtual comm ports are "working properly".
I've double checked the connections being made between the MSP-FET and the custom pinout 10-pin connector for the target (MSP430F5308) using the appropriate TI documentation, done a continuity check between both ends of that custom cable I created, and verified that in each of the two cases the MSP430 processors appear to still be up and running.
Unless I did something accidentally, neither processor was secured such that the JTAG interface was disabled. Is there any case where something like this could occur?
Thank you very much.