This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
I'm trying to use my launchpad board with the firmware I downloaded from the MCT8329 EVM webpage. I want to use my launchpad to connect with the mct8329 in order to use the GUI config tool. But it's getting stuck on the CS_initFLL function, specifically in this while:
Hi Axel
could you please check if the code is the same with https://www.ti.com/tool/download/SLAC807
For DCO and FLL clock setting, please refer to msp430fr235x_CS_02.c code on https://www.ti.com/tool/download/SLAC740
Thanks!
Hi, the code is different than the one I got from the MCT8329EVM page and it's actually working with the GUI for the MCT8316 GUI but I'm using a different IC.
Hi Axel
For isolate this issue, could you please check MSP430FR2355 DCO and FLL using the CS example code?
Thanks!
Hi Axel
Could you please compare the FLL setting code and execution result between the example code and the code from CS_initFLL function?
Please consider update the CS_initFLL code and check if the "stuck" issue can be solved.
Thanks!
**Attention** This is a public forum