Part Number: MSP430F6775A
Tool/software:
Hi,
I would like to ask, If I store values from any register like module in the start of main program or in system_pre_init() funtion into an array shouldn't be the value the same as default defined in the user guide? I mean the default configuration loaded by the bootcode in the hidden partition should match the stored configuration or not? If I did not modified any register yet of course. And also may be the configuration read from that location different than what debugger says during debugging when jtag is used? I don't mean the registers which are used by the debuging module. I mean I did so and in some cases they are different like the FLLD part of UCS seems to have a zero there instead of one which should be default according to UG. And I am wondering what could be wrong.
Thank you for your answer.