This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2633: Capacitive touch sensitivity

Part Number: MSP430FR2633

Tool/software:

We are building a product called Smart Lock where multiple modules like touch, NFC, finger print, and much more are present.

We have built the custom touch control board using MSP430FR2633IRHBR.

If we place our finger on the PCB PADs, we are able to detect. We have added the transparent acrilyic sheet to the PCB, and we are able to sense it. but if we add the actual panel, which has the black coating, we are unable to detect the touch sensitivity.

Can anyone suggest if there is any way to increase the sensitivity?

Attached the product panel & PCB

Custom PCB

our product panel

  • Hello Tejas,

    Does the black panel contain any conductive paint or coatings?

  • its just coating

  • Hi Tejas,

    If we place our finger on the PCB PADs, we are able to detect. We have added the transparent acrilyic sheet to the PCB, and we are able to sense it.

    When you tested this with the acrylic sheet, did you simply lay the sheet on top of the keypad, or use some type of adhesive so that the sheet was in direct contact with the pads?  This is good because it minimizes any air gap between the acrylic and the pads (sensors).

    but if we add the actual panel, which has the black coating, we are unable to detect the touch sensitivity

    And when you placed the actual panel, does it rest on top of the pads (sensors) just like the acrylic sheet, with no air gaps?  Reason I ask is any air gap will drastically reduce sensitivity.

    BTW, what is the thickness of the acrylic sheet and the actual panel?

    Do you have the ability to send data from the MSP430FR2633 to the Captivate GUI?

  • Yes, We connected the IC with the GUI and altered the threshold and capacitive parameters and the issue got resolved

**Attention** This is a public forum