This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430I2041: when the power factor is 0.5, the measurement result deviation is 0.5

Part Number: MSP430I2041


Tool/software:

In the measurement of electric meters, comparing the MSP430I2041 with the calibration free measurement chip, it was found that the measurement result error of MSP430I2041 is relatively large when the power factor is less than 0.9. For example, when the power factor is 0.5, the measurement result deviation is 0.5; Can you provide suggestions on what may have caused the current results?

**Attention** This is a public forum