Tool/software:
We are inputting a 100kHz sin wave from 800mV to 1V and trying to see the resulting output from the ADC. For some reason, we can get a clean output very rarely, and even then the frequency does not match. What could be the problem? The figure on the left is how it looks usually and in the following figures there is a short burst of a clean output.
Thank you for the response! We applied a 100kHz sin wave from 400mV to 600mV and we got a similarly noisy result. The register level SDHS example code for the MSP430FR6043 stated that the valid input range was 600mV to 1.2 V, how did they arrive at that input range? We are still unsure what is causing the noise. The frequency of the output also seems to be slightly off as well. For the python script we are using to plot the results, we set the sampling frequency as 8 MHz because of the 8 Msps output for the SDHS, is this correct? The code we have currently for the SDHS ADC is attached to this reply.
/* --COPYRIGHT--,BSD * Copyright (c) 2017, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * --/COPYRIGHT--*/ //****************************************************************************** // sdhs_ex1_8msps_sampling.c - SDHS sampling at 8MSPS and DTC transfer results to RAM // // Description: Configure the SDHS for stand-alone use (register mode) at 8MSPS. // Use the DTC to transfer the results to an array in RAM. // // MSP430FR6047 // --------------- // /|\| | // | | | // --|RST | // | P1.0|---> LED // | |-USSXTIN // | |-USSXTOUT // | CH0_IN|<--- input signal // // Wallace Tran // Texas Instruments Inc. // June 2017 //****************************************************************************** #include "driverlib.h" #include "sdhs.h" #include <stdio.h> #include <stdint.h> #if defined(__TI_COMPILER_VERSION__) #pragma DATA_SECTION(results, ".leaRAM") #pragma RETAIN(results) uint16_t results[1024] = {0}; #elif defined(__IAR_SYSTEMS_ICC__) #pragma location = 0x2C00 __no_init uint16_t results[1024]; #pragma required = results #elif defined(__GNUC__) uint16_t results[1024] __attribute__ ((section(".leaRAM"), used)); #else #error Compiler not supported! #endif #define RESULTS_SIZE 256 // Assuming 256 samples #define FULL_SCALE_VOLTAGE 0.755f #define GAIN 1.01158f // Approximation of 10^(0.1/20) #define BIAS 0.9f #define MAX_ADC_VALUE 2047.0f #define RAM_END_ADDRESS 0x6000 //volatile int16_t *r = (int16_t *)0x4000; volatile uint8_t adc_data_ready = 0; // Global flag float voltage; int16_t adc_code; static uintptr_t current_ptr = 0x4000; int16_t *end_ptr = (int16_t *)RAM_END_ADDRESS; volatile uint8_t LEA_RAM_SDHS_RESET_FLAG = 0; // void display_adc_values() { // int i; // for (i = 0; i < RESULTS_SIZE; i++) { // if (current_ptr >= RAM_END_ADDRESS) { // printf("Reached end of RAM, resetting pointer.\n"); // LEA_RAM_SDHS_RESET_FLAG = 1; // current_ptr = 0x4000; // Reset to start of RAM // } // adc_code = (*(int16_t *)current_ptr) >> 4; //12 bits stored into one 16 bit word // voltage = (adc_code * (FULL_SCALE_VOLTAGE / 2)) / (GAIN * MAX_ADC_VALUE) + BIAS; // //printf("ADC[%d]: Code = %d, Voltage = %.3f V\n", i, adc_code, voltage); // current_ptr += 2; // Move to the next 16-bit value // } // } void main (void) { //Stop WDT WDT_A_hold(WDT_A_BASE); //PA.x output GPIO_setAsOutputPin(GPIO_PORT_PJ, GPIO_PIN1); //Disable the GPIO power-on default high-impedance mode to activate previously configured port settings PMM_unlockLPM5(); // //Set all PA pins HI // GPIO_setOutputHighOnPin( // GPIO_PORT_PJ, // GPIO_PIN1 // ); /*Clock Setup*/ FRAMCtl_A_configureWaitStateControl(FRAMCTL_A_ACCESS_TIME_CYCLES_1); //necessary for clock operating above 8MHz //Set Divider to 4 before changing frequency to prevent out of spec opreation from overshoot transient CS_initClockSignal(CS_ACLK, CS_VLOCLK_SELECT, CS_CLOCK_DIVIDER_4); CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_4); CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_4); //Set DCO to 16 MHz and wait for DCO to settle CS_setDCOFreq(CS_DCORSEL_1, CS_DCOFSEL_4); //rsel: 0 = low, 1 = hi; fsesl6: low = 5.33MHz, hi = 16MHz __delay_cycles(60); //(10 us / (1/4MHz)) + 20 cycles // Set all dividers to 1 for 16MHz operation // MCLK = SMCLK = 16MHz CS_initClockSignal(CS_ACLK, CS_VLOCLK_SELECT, CS_CLOCK_DIVIDER_1); CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1); CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1); /*End of Clock Setup*/ /*Setup SAPH for Register Mode*/ SAPHKEY = KEY; SAPHBCTL &= ~ASQBSC; SAPHBCTL |= CPDA; SAPHICTL0 = 0; SAPHKEY = KEY+1; /*end of SAPH Setup*/ /*Initialize HSPLL*/ //Configure USSXT Oscilator to operator at 8MHz HSPLL_xtalInitParam xtalParam; xtalParam.oscillatorType = HSPLL_XTAL_OSCTYPE_XTAL; xtalParam.oscillatorEnable = HSPLL_XTAL_ENABLE; xtalParam.xtlOutput = HSPLL_XTAL_OUTPUT_ENABLE; HSPLL_xtalInit(HSPLL_BASE, &xtalParam); // Check if oscillator is stable while(HSPLL_getOscillatorStatus(HSPLL_BASE) == HSPLL_OSCILLATOR_NOT_STABILIZED); //set up timer to wait for crystal to stabilize: 4096 clocks for crystal resonator --> For 8MHz XTAL, 4096 clocks = 512us. Using VLO = 9.4kHz, wait 5 timer clock cycles = 532us Timer_A_initUpModeParam timerParam = {0}; timerParam.timerPeriod = 5; timerParam.captureCompareInterruptEnable_CCR0_CCIE = TIMER_A_CCIE_CCR0_INTERRUPT_ENABLE; // Timer sourced from ACLK (VLO) timerParam.clockSource = TIMER_A_CLOCKSOURCE_ACLK; // Clear timer timerParam.timerClear = TIMER_A_DO_CLEAR; timerParam.startTimer = true; Timer_A_initUpMode(TA4_BASE, &timerParam); //Timer A4 -- disable interrupts after waiting for crystal to stabilize // Enter LPM3 w/interrupts enabled __bis_SR_register(LPM3_bits | GIE); // For debugger __no_operation(); //Initilize PLL HSPLL_initParam hspllParam; hspllParam.multiplier = PLLM_19_H; //multiply by 19 to get desired 80 MHz output clock frequency: 80MHz x 2 = 8MHz x (19+1) hspllParam.frequency = HSPLL_GREATER_THAN_6MHZ; //HSPLL will be greater than 6 MHz HSPLL_init(HSPLL_BASE, &hspllParam); //Power up UUPS to start PLL and wait UUPS_turnOnPower(UUPS_BASE, UUPS_POWERUP_TRIGGER_SOURCE_USSPWRUP); while(UUPS_getPowerModeStatus(UUPS_BASE) != UUPS_POWERMODE_READY); //wait for UUPS to power up while(HSPLL_isLocked(HSPLL_BASE) == HSPLL_UNLOCKED); //wait for PLL to lock /*End of HSPLL Configuration*/ /*Setup SDHS (Sigma-Delta High Speed ADC)*/ SDHS_initParam sdhsParam = {0}; //create config struct //All SDHS parameters, brief descriptions and defaults are commented sdhsParam.triggerSourceSelect = SDHS_REGISTER_CONTROL_MODE; // Trigger source select - SDHS_REGISTER_CONTROL_MODE //sdhsParam.msbShift = SDHS_NO_SHIFT; // Selects MSB shift from filter out - SDHS_NO_SHIFT //sdhsParam.outputBitResolution = SDHS_OUTPUT_RESOLUTION_12_BIT; // Selects the output bit resolution - SDHS_OUTPUT_RESOLUTION_12_BIT sdhsParam.dataFormat = SDHS_DATA_FORMAT_TWOS_COMPLEMENT; // Select data format - SDHS_DATA_FORMAT_TWOS_COMPLEMENT sdhsParam.dataAlignment = SDHS_DATA_ALIGNED_LEFT; // Selects the data format - SDHS_DATA_ALIGNED_LEFT //sdhsParam.interruptDelayGeneration = SDHS_DELAY_SAMPLES_1 ; // Selects the data format - SDHS_DELAY_SAMPLES_1 sdhsParam.autoSampleStart = SDHS_AUTO_SAMPLE_START_DISABLED; // Selects the Auto Sample Start - SDHS_AUTO_SAMPLE_START_DISABLED sdhsParam.oversamplingRate = SDHS_OVERSAMPLING_RATE_10; // 80MHz / 10 (OSR) = 8 MSPS; MCLK must be >= 8 MHz - SDHS_OVERSAMPLING_RATE_10 //sdhsParam.dataTransferController = SDHS_DATA_TRANSFER_CONTROLLER_ON; // Selects the Data Transfer Controller State - SDHS_DATA_TRANSFER_CONTROLLER_ON //sdhsParam.windowComparator = SDHS_WINDOW_COMPARATOR_DISABLE; // Selects the Window Comparator State - SDHS_WINDOW_COMPARATOR_DISABLE //sdhsParam.sampleSizeCounting = SDHS_SMPSZ_USED; // Selects the Sample Size Counting - SDHS_SMPSZ_USED // Initialize SDHS module SDHS_init(SDHS_BASE, &sdhsParam); //initilzie SDHS based on above parameters SDHS_setTotalSampleSize(SDHS_BASE, 256); //Set to 256 samples SDHS_setPGAGain(SDHS_BASE, 0x19); //PGA Gain of 0.1 dB SDHS_setModularOptimization(SDHS_BASE, SDHS_OPTIMIZE_PLL_OUTPUT_FREQUENCY_77_80MHz); //Using 80 MHz PLL so optimize for 80 MHz SDHS_setDTCDestinationAddress(SDHS_BASE, 0); //Set destination address as the start fo LEA RAM for the DTC (Data Transfer Controller) SDHS_enableInterrupt(SDHS_BASE, SDHS_ACQUISITION_DONE_INTERRUPT); //Enable the aquisition done interrupt (i.e. after 256 samples are transferred) //enable acquisition done interrupt SDHS_enableTrigger(SDHS_BASE); //Allow system to react to event SDHS_enable(SDHS_BASE); //turn on SDHS_startConversion(SDHS_BASE); //Start conversion __delay_cycles(320); //Delay for worst case PGA settling time: 40 us = 1/(8MHz) * 320 /* ---Begin configure TA2.1 for 1/sec to trigger the pulse generation and toggle LED--- */ Timer_A_initUpModeParam timerParam2 = {0}; timerParam2.timerPeriod = 9400; //timerPeriod in clock cycles, 9400 cycles / (9.4 kHz) -> 1 s TA2CCR1 = 4700; //interrupt occurs 0.5 s --> enter routine at frequency of 2 Hz --> GPIO toggles at frequency of 1 Hz TA2CCTL1 = OUTMOD_7 | CCIE; // Enable output signal to trigger PPG, enable interrupt // Timer sourced from ACLK (VLO) timerParam2.clockSource = TIMER_A_CLOCKSOURCE_ACLK; //VLO has frequency of 9.4 kHz from page 42 of data sheet // Clear timer timerParam2.timerClear = TIMER_A_DO_CLEAR; timerParam2.startTimer = true; Timer_A_initUpMode(TA2_BASE, &timerParam2); /* ---End configure TA2.1 for 1/sec to trigger the pulse*/ /*Timer A.0 Setup for Toggling GPIO PJ.1 configure Timer0_A -- Toggling GPIO PJ.1 Timer_A_initUpModeParam upConfig = {0}; upConfig.clockSource = TIMER_A_CLOCKSOURCE_SMCLK; upConfig.clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_4; //set TimerA0 to SMCLK/4 = 4MHz upConfig.timerPeriod = 10000; //each # is 500ns upConfig.timerInterruptEnable_TAIE = TIMER_A_TAIE_INTERRUPT_DISABLE; //disable overflow interrupt upConfig.captureCompareInterruptEnable_CCR0_CCIE = TIMER_A_CCIE_CCR0_INTERRUPT_ENABLE; //enable CCR0 interrupt upConfig.timerClear = TIMER_A_DO_CLEAR; initialize Timer0_A Timer_A_initUpMode(TIMER_A0_BASE, &upConfig); enable Timer0_A0 interrupt __enable_interrupt(); //do i need this??? start Timer0_A Timer_A_startCounter(TIMER_A0_BASE, TIMER_A_UP_MODE); */ while(1){ //Enter LPM0 w/interrupts enabled // if (adc_data_ready) { // adc_data_ready = 0; // Clear flag // display_adc_values(); // updates global variables for debug: voltage, adc_code, and current_ptr // } __bis_SR_register(LPM0_bits | GIE); //For debugger __no_operation(); } } // Timer A2 interrupt service routine #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = TIMER2_A1_VECTOR __interrupt void Timer2_A1_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(TIMER2_A1_VECTOR))) Timer2_A1_ISR(void) #else #error Compiler not supported! #endif { switch(__even_in_range(TA2IV, TAIV__TAIFG)) { case TAIV__NONE: break; // No interrupt case TAIV__TACCR1: SDHS_endConversion(SDHS_BASE); // if(LEA_RAM_SDHS_RESET_FLAG){ // LEA_RAM_SDHS_RESET_FLAG = 0; // SDHS_disable(SDHS_BASE); // SDHS_disableTrigger(SDHS_BASE); // SDHS_setDTCDestinationAddress(SDHS_BASE, 0); // SDHS_enableTrigger(SDHS_BASE); // SDHS_enable(SDHS_BASE); // } SDHS_startConversion(SDHS_BASE); // Start conversion break; case TAIV__TAIFG: break; // overflow default: break; } } // SDHS interrupt service routine #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = SDHS_VECTOR __interrupt void SDHS_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(SDHS_VECTOR))) SDHS_ISR(void) #else #error Compiler not supported! #endif { switch(__even_in_range(SDHSIIDX, IIDX_6)) { case IIDX_0: break; // No interrupt case IIDX_1: break; // OVF interrupt case IIDX_2: // ACQDONE interrupt GPIO_toggleOutputOnPin(GPIO_PORT_PJ, GPIO_PIN1); // Toggle GPIO J.1 to show new cycle //adc_data_ready = 1; __delay_cycles(1000); // 10000 / 16*10^6 = 625 us delay? __no_operation(); //put breakpoint here to view results --> 1V would result in 1240 if reference voltage is 3.3 V for a 12-bit ADC break; case IIDX_3: break; // SSTRG interrupt case IIDX_4: break; // DTRDY interrupt case IIDX_5: break; // WINHI interrupt case IIDX_6: break; // WINLO interrupt default: break; } //LPM0_EXIT; } // Timer A4 interrupt service routine -- Stabilize USSXT #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = TIMER4_A0_VECTOR __interrupt void Timer4_A0_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(TIMER4_A0_VECTOR))) Timer4_A0_ISR(void) #else #error Compiler not supported! #endif { // Stop the timer and wake up from LPM Timer_A_startCounter(TA4_BASE, TIMER_A_STOP_MODE); //Stop Timer 4 __bic_SR_register_on_exit(LPM3_bits | GIE); //Disable gloabal interrupts for the rest of SDHS configuration -- will be enabled again in the main loop. __no_operation(); } // /* // // Timer0_A0 interrupt service routine // #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) // #pragma vector = TIMER0_A0_VECTOR // __interrupt void Timer0_A0_ISR (void) // #elif defined(__GNUC__) // void __attribute__ ((interrupt(TIMER0_A0_VECTOR))) Timer0_A0_ISR (void) // #else // #error Compiler not supported! // #endif // { // Timer_A_clearCaptureCompareInterrupt(TIMER_A0_BASE, TIMER_A_CAPTURECOMPARE_REGISTER_0); // GPIO_toggleOutputOnPin(GPIO_PORT_PJ, GPIO_PIN1); // } // */
We applied a 100kHz sin wave from 400mV to 600mV and we got a similarly noisy result. The register level SDHS example code for the MSP430FR6043 stated that the valid input range was 600mV to 1.2 V, how did they arrive at that input range?
One from my side is PGA input range limitation.
The 600mV to 1.2V is for SDHS input range limitation.
Here is the signal chain:
Signal -> PGA -> SDHS -> MSP430's RAM.
We are still unsure what is causing the noise.
Nether do I. Could you please try to change the MSP430 chips or the ultrasonic sensor transducer?
we set the sampling frequency as 8 MHz because of the 8 Msps output for the SDHS, is this correct?
Where is this sampling frequency? If in the software signal processing function, this fs need to keep same as ADC sampling rate.
**Attention** This is a public forum