Part Number: MSP430G2553
Other Parts Discussed in Thread: MSP-EXP430G2ET, , LP-MSP430FR2476, MSP-FET, MSP430FR6989
Tool/software:
Hello,
I just received a new MSP-EXP430G2ET LaunchPad kit with an MSP430G2553 MCU. When I tried flashing the "MSP-EXP430G2ET - LaunchPad Out Of Box Demo" in CCS 20.1.0 it asked me to update which failed with the error below. Now it needs recovery, which also fails. I've tried recovery with CCS the MSP Flasher and the FET-Pro430 by Elprotronic, but all fail. I have the same problem with two different MSP430FR boards, which failed to update and can't be recovered. I thought buying a newer board would fix this, but apparently not. The LP-MSP430FR2476 updated without a problem and I've tried on a different system, so I believe there is no issue with my setup.
I now have three bricked boards by using TI's software, I hope you can help me.
Error in CCS:
MSP430: Error initializing emulator: A firmware update is required for the MSP430 Debug Interface (MSP-FET430UIF / MSP-FET / eZ-FET). Click the "Update" button to update the firmware and launch your debug session (this may require several update steps). DO NOT UNPLUG THE INTERFACE DURING THE UPDATE.
MSP430: Error: MSP-FET / eZ-FET core(communication layer) update failed
MSP430: Error initializing emulator: One of the connected MSP-FETs / eZ-FETs debuggers needs recovery. Select 'Recover' to start the recovery process. Note: Only one MSP-FET / eZ-FET debugger can be connected to your system during recovery.
MSP430: Error: MSP-FET / eZ-FET recovery failed