This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6047: How can I find Water Flow Demo CCS examples code?

Part Number: EVM430-FR6047


Tool/software:

Hello, I want to use the EVM430-FR6047 board to transmit the water flow sensor value to another Arduino board via serial communication.
But I still can't find the source for the Water Demo project.

The only way I found was to upload the MSP430FR6047EVM_USS_Water_Demo_LPM_02_40_00_00.txt image to the EVM430 board using the UniFlash 9.1.0 program.
However, it seems that this method will not allow you to modify the program to CCS 20.1.0.

So I'm wondering, is there an example of a CCS project that gets the Water Flow sensor values?
If not, I would appreciate it if you could give me some titles of examples that I can refer to.
 
Thank you for all your help and have a nice day.
 

**Attention** This is a public forum