This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-GANG: Error 23, 33 occurs while using the MSP430FR5968

Part Number: MSP-GANG
Other Parts Discussed in Thread: MSP430FR5968, MSP-FET

Tool/software:

Hi experts,

My customer has created a board using MSP430FR5968, but there are cases where it cannot be written from MSP-GANG.
Q1: Could you tell me the cause and solution? 
Q2:Are the write specifications different between MS-FET and MSP-GANG?

[Details]

  • Writing is possible if they use MSP-FET.
  • With MSP-GANG, the first writing is successful, but Error-23 or Error-33 occurs after multiple tries.
  • The power is supplied from the debugger at 2.3V.
  • MSP-GANG uses an external power supply of 9V/1A.
  • The result does not change even if the cable is changed.
  • The result does not change GUI and standalone mode.

The GUI setting screen and version information are shown below.

The circuit diagram is shown below.

  • Note: Again, writing is possible if they use MSP-FET.
  • They disconnected VCC_TARGET and connected only VCC_TOOL, but the result did not change.
  • They removed the reset IC, but the result did not change.
  • The results don't change even if I remove the 2M resistor.

Best regards,
O.H

**Attention** This is a public forum