This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5969-SP: Maximum SPI Clock Frequency

Part Number: MSP430FR5969-SP

Tool/software:

Hi,

I wanted to confirm that the maximum SPI clock frequency is 16MHz and can only be sourced by the SMCLK.

According to the datasheet, it can be sourced by SMCLK or ACLK, but it looks like ACLK maximum is much lower, so the only option for 16MHz is to use the SMCLK.

Is that correct?

Thanks!

**Attention** This is a public forum