Part Number: MSP430F5659
Tool/software:
Hello TI Community,
I'm developing a custom bootloader for the MSP430F5659 microcontroller. I've set up my project as follows:
Current Implementation:
- Created two separate projects: one for the bootloader and one for the application
- Modified the bootloader's linker script to:
- Start address: 0x8000
- Size: 4KB
- Modified the application's linker script to:
- Size: 28KB
- Basic functionality: The bootloader blinks an LED rapidly 3 times, then jumps to the application code start address
Questions I'm struggling with:
- Reset Vector Configuration: What modifications are needed for the reset vector when implementing this dual-image architecture? Since I have both a bootloader and application code, I'm unsure how to properly handle the reset vector to ensure correct system initialization.
- Proper Flashing Procedure: What is the correct procedure for flashing both projects onto the device? Should I flash them separately or combine them into a single image? Are there specific considerations for preserving the bootloader when updating the application code?
Has anyone implemented a similar setup with the MSP430F5659? Any examples, code snippets, or documentation references would be greatly appreciated.
I've also added Memory Organization of MSP430F5659 below.