This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2522: Application issues.

Expert 2320 points

Part Number: MSP430FR2522

Tool/software:

Hi Team,

The connection between the control board and the touchpad is two separate boards,
Connect through 40mm FFC wire. Is this plan feasible?

  • Hi Reed,
    Let me consult with my team about this.

    Best Regards,

    Diego Abad

  • Hi Reed,
    The plan seems feasible. However, you should be aware that the TX and RX signals should be separated from each other through the FFC. In your cable connections, consider including some ground lines between your TX and RX signals in the FFC cable. Suppose you must have other digital signals in the cable. The recommendation is to either place them between ground lines or near the TX lines, as they are less susceptible to interference. For more information, please refer to the Mutual Capacitance Traces section of the CapTIvate Technology Guide.


    Best Regards,
    Diego Abad

**Attention** This is a public forum