Tool/software:
I am evaluating to Migration From the Non-A MSP430F67xx Devices to the MSP430F67xxA Devices
From TI application note (SLAA666A) said below.
"Migration From the Non-A MSP430F67xx Devices to the MSP430F67xxA Devices
To migrate from a non-A MSP430F67xx device to its corresponding MSP430F67xxA device, minimal
changes are necessary. A MSP430F67xx device and its corresponding MSP430F67xxA device are pin-topin
compatible, so a non-A chip can physically be replaced with an A version. Additionally, the software on
a MSP430F67xx device should also run on a MSP430F67xxA device as long as the software is updated
to correspond to the proper header files and device name in the IDE project settings."
I have another question about using our .r43 library for metrology and communication protocol (IAR MSP430 compiler).
Is it necessary to recompile for the .r43 library (since the MCU memory address and structure seem to not need to be recompiled)?
Thank you,