Other Parts Discussed in Thread: MSP430F5510, MSP-FET
Hello,
I am looking to test the onchip USB BSL feature of the device thru' hardware method as described in SLAA452b,Page 2 . At the beginning i don't want to go with Custom
Flash Based BSL design
Crystal on the board is 25 MHz (X2).I have coded a small project which doesn't have any code related to USB.
The device is power by external LDO ( LDO powered from usb VBUS supply ). USB interfacs h/w is as per app note slaa452b .Instead of a switch I have shorted the
PUR and VUSB thru' 100 Ohm.
I have open up the firmware update utility and connected the PC USB connector to device.
I got a pop-up message on PC saying Device not recognized i.e means PC (host) detected a USB device but in enumeration process it didn't get a suitable driver to load.
But as MSP430 reports itself as a HID device should it n't be recognized ??
How do i get the TI's on chip usb bsl tested ?
where did i go wrong ??
Regards,
Ars