Part Number: MSP430FR6047
Other Parts Discussed in Thread: EVM430-FR6047
Tool/software:
Hi,
On EVM-MSP430FR6047 when I set Signal sampling frequency = 4 MHz,
Over sampling rate = 20
then it works fine and also communicates using USS design center tool. Fine enough.
But when I set
Signal sampling frequency = 8 MHz,
Over sampling rate = 10.
It stops communicating using USS design center tool. You click on ADC capture but no communication, also no waveform capture is happening.
Also you cannot update the configuration values. Why?
Even after power off board will not communicate. Then again flash the firmware and it starts working.
Thanks,
Anup Kumar.