Other Parts Discussed in Thread: MCF8315C, MSPM0G3507
Tool/software:
Hello Ti,
I have few questions regarding LP-MSPM0G3507, and Sensorless FOC for PMSM example in SDK,
-Does the algorithm compensate for the change in motor resistance during runtime and if not, how can i measure and update resistance in runtime? i am not sure if i updated it in the pUserInputRegs it will be considered by the calculations or values already captured at the init. phase.
-Comparing this SDK software implementation to the HW solution based on MCF8315C does the HW version compensate for this resistance change?
-In case of using MSPM0G3507 and SDK, motor is rotating and switching to closed loop ok but if loaded only run in open loop and when switch to closed loop it is very slow or rotate for while then stops. while it works fine with this load and higher loads when using the HW version (MCF8315). what do you suggest to tune / monitor? i tried open/closed loops current limits, acceleration parameters and Handoff threshold.
Regards