Tool/software:
Hi,
I could use some help on whether I can expect to use the TIA on the launchpad.
1) does the EXFET use these pins normally or only in certain modes? if I direct to only use SWD how do I direct the tool to only use that?
2) So, assuming I get the registers programmed to what I need and launch the code, then I could or should or would need to remove the shorting blocks J101-5:6, J101-3:4 ??
3) considering I will be trying to assess photodiode and TIA performance using this board. After initial validation of function, would/should I cut 'extraneous" traces to avoid stray capacitance? Trying to keep capacitance minimal of course - just on P1.6 P1.7 as they branch to J101.
THANKS FOR HELPING!