This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR59941: MSP430FR59941

Part Number: MSP430FR59941

Tool/software:

I have a blank (not programmed) unit and I would like to test it by reading device ID of the device. 

As I understood the I2C address is 0x48 and the register address is 0x01A04. Is this right?

My questions are:

  1. what pins I can communicate with the device via I2C? As I see in the datasheet there are 4 I2C channels, UCB[0-3]. Can I use all of the channels, or I need any strapping or configurations?
  2. After writing 0x48 will I receive ACK or NACK?
  3. Can I write immediately the 0x01A04 or I need to write byte by byte and wait for ACK? I mean write 0x1A get ACK and then 0x04 and get ACK.
  4. How I read the data? It is the same byte -> ACK -> byte

**Attention** This is a public forum