This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F1111A: Program burning issue

Part Number: MSP430F1111A

Tool/software:

Dear TI Engineer,

We have used MSP430F1111AIDWR in one of our projects, and it was used normally before. However, during the production of this batch, we encountered a problem of program burning, with a defect rate of 8%.

The schematic is as below:

The program burning port is J4, and its connection pins with MSP430F1111AIDWR are shown in the table below.

J4 port MSP430F111AIDWR
1(TST) PIN1(TST)
2(TDO) PIN20(TDO)
3(TMS) Not use
4(TCK) Not use
5(RST/NMI) PIN7(RST/NMI)
6(GND) PIN4(GND)
7(VCC) Not use(Powered by external 3V)
8(TDI) Not use

We attempted a cross experiment and found that the program burning issue followed the chip. Do you have any suggestion for this issue?

Thanks,

Kind Regards

**Attention** This is a public forum