This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5043: Recommended DToF option differences

Part Number: MSP430FR5043


Tool/software:

Hi Expert

Could you please share the "Recommended DToF option" differences between <0.5usec and >= 0.5usec is there the accuracy loss?

 

Thanks

Joe

  • Hi Joe,

    There are two options here due to the development history of the USS library. In the earlier version of USS library, it can only handle a flow rate within (+- 0.5*transducer period) which is called USS_Alg_dToF_Calculation_Option_water. And later on, the algorithm upgraded and can solve a flow rate without the limitation which is called USS_Alg_dToF_Calculation_Option_estimate. It only improves the ability to deal with high flow rate, no impact on the accuracy. 

    Best regards,

    Cash Hao

**Attention** This is a public forum