I am using the MSP-GANG430 in standalone mode. To verify that the image being burnt onto the targets in production matches the approved hex code I would like to be able to read the image data from the gang programmer via the RS232 port. I cannot burn the code onto a target then read the target memory because the target is put into "Secure Device" mode. Any assistance would be appreciated. Thanks