This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5132: MSP430F5132

Part Number: MSP430F5132
Other Parts Discussed in Thread: TIDA-00121,

Tool/software:

 Integration of a Remote Monitoring system (RMS)into the TIDA-00121 reference design, utilizing the MSP430F5132 microcontroller along with a PIR motion control sensor.

  • Remote Monitoring System (RMS): The charge controller should be provided with a communication node with necessary cables and connectors to interface with the charge controller and a monitoring system enable it to monitor the location and status of system online with app as per remote Monitoring System.                                                                                                                                                           REMOTE MONITORING SYSTEM The Smart Solar Street Lighting System shall automatically connect directly to the public mobile network via 2G/3G/4G/SG or any latest technology networks for sending data to cloud server or CMS (Central monitoring System) via RMS hardware. The remote monitoring system shall collect and centrally send real-time performance data (including equipment failures) for each Smart SSLS (Solar Street Lighting System). RMS hardware shall be installed in every luminary and shall be capable to generate report for functionality, issues, healthiness, problem status etc. to the RMS Cloud Server with the help of GSM module attached& Network Coverage which shall be updatable OVER THE AIR (OTA) during the contract period. All the communication of RMS device with the controller circuit. RMS must follow Government of India MNRE specifications as applicable. The executing agency shall ensure that the supplied RMS Device should be hackproof and leak proof to avoid the malicious activity or event. The communication nodes shall connect to the charge controller through suitable communication interface and automatically sense and monitor various parameters of the Solar Street Light. The RMS dashboard are as follows:
  • Battery Parameter’s:

Battery Voltage (BV)

  • Battery Current (BI)
  • Battery Power (BP)
  • Solar PV Parameters:
  • Solar PV Voltage (SV)  
  • Solar PV Current (SI)
  • Solar PV Power (BP)
  • Load Parameters:
  • Load Voltage (LV)
  • Load Current (LI)
  • Load Power (LP)
  • Load ON OFF condition
  • System shutdown due to fault (even fault should be recorded)
  • Following Parameters to be displayed in the dashboard of the RMS software (GUI/web user interface:

Sr. no.

Parameter to be monitored

1

Device ID-IMEI

2

Serial no, of Light

3

Battery Voltage

4

Battery Current

5

Battery Power

6

Solar Module Voltage

7

Solar Module Current

8

Solar Module Power

9

Luminary Voltage

10

Luminary Current

11

Luminary Power

12

System Status (Green-ok RED-not ok)

13

Battery Fault

14

Module Fault

15

Luminary fault

16

Battery Fault Date

17

Module fault Date

18

Luminary fault Date

19

Luminary fault Time

20

Luminary ON time

21

Luminary OFF time

22

Fault time date

23

Fault rectification date

24

Brightness Level

25

Full Brightness Hour

26

Half Brightness Hour

27

Harvested energy

27

Battery State of Charge (%)

27

Battery Depth of Discharge (%)

Please guide me for this in same project.

**Attention** This is a public forum