Part Number: MSP430FR6047
Tool/software:
Hi,
What If I enables #ifdef USS_APP_AGC_CALIBRATE_ENABLE in code.
where it can impact my calculation of time of flight?
Regards,
Anup Kumar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR6047
Tool/software:
Hi,
What If I enables #ifdef USS_APP_AGC_CALIBRATE_ENABLE in code.
where it can impact my calculation of time of flight?
Regards,
Anup Kumar
Hi,
The AGC(auto gain calibration) function is used to calibrate the PGA gain setting to always keep the maximum ADC capture signal level at a certain number. It does not directly impact the calculation of TOF.
Best regards,
Cash Hao
Thanks for your reply,
So, can I use this at run time when I am calculating the Flow rate?
Also, I have seen in the code if you are measuring the flow rate at say every 1 second and if I set calibration interval to 60, then does it mean that after every 1 minute it will calibrate/adjust the gain?
In code it is hard coded that 3dB value of 2^11 (12-bit ADC) that is around 1449. Is this value works as reference point for AGC gain calibration?
Regards,
Anup Kumar
Hi,
You can use it at run time.
And yes, it means calibrating every 1 minute. You can decide the interval as you needed.
For 3rd question, you can refer to below image.

Best regards,
Cash Hao
**Attention** This is a public forum