Tool/software:
Using 2% in the error equation does not give you the equivalent of a 2% change in the voltage divider,
of the two method which one is correct?

my question is a follow up from my previous thread:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Using 2% in the error equation does not give you the equivalent of a 2% change in the voltage divider,
of the two method which one is correct?

my question is a follow up from my previous thread:
Hi Jonathan,
You are correct and I was seriously wrong. My apologies. Thank you for catching this and I will update the original posting.
So yes, when changing only one resistor at a time by +/-1% in the voltage divider, the resulting vout will not change by +/-1%, but rather roughly +/- 0.5%. And of course this would change if the two resistors where different values to begin with, like a 330K and 100K.
Again sorry for the confusion on this.
Hi,
Thank you, I'm looking forward to the response.
Please show how the +/-1% in the voltage divider will result in the Vout change roughly of +/- 0.5%
Thanks
Hi Jonathan,
Ok, here is screen shot of calculations (spreadsheet attached)
When R1 = R1 + 1%, R2 = R2, Vout changes by -0.498% (0.00498).
When R1 = R1 + 1%, R2 = R2 - 1%, Vout changes by -1.0%.
Does this help?
Hi Dennis,
based on the attached spreadsheet, is it correct to conclude that you must always calculate voltage divider percentage error?
for example if R1 and R2 are not equal ,the error for 1% resistors does not equal a 1% Voltage divider percentage error
Can you provide an updated total ADC error using Vout change % for resistor tolerance at 3% ,
taking into account Vref error of 1.5%,2 LSB error for 10 bit ,vout change % due to resistor tolerances and any other eror that i may have missed

7416.R_divider_percent_error_calc 20250820.xlsx
Regards
Jonathan Kabangu
Hi Jonathan,
is it correct to conclude that you must always calculate voltage divider percentage error?
I would say if you want a true worse case error for your measurements, then yes, you must include all sources of error. ADC error, Vref error, and R divider error.
Ignoring the error in the voltage divider I would think is important to consider. I see from earlier post you are measuring 12 v or 24 v. How important is it to accurately measure 12v or 24v? What precision is required?
I don't know what you ultimately do with the measurement but would a 3% error cause your system to now work?
If you agree with how the errors are calculated, and using the calculations you added to the spreadsheet (BTW thanks for the contribution) then calculating the measurement error due to 3% error in the resistors, I leave this exercise to you. ;)
**Attention** This is a public forum