Tool/software:
Hi,
As per datasheet it says i cannot connect more than 2.2nF and 47K as external RC for Reset.
My VCC rise is around 0.2ms and i need my reset to rise after 1ms as i cannot increase value of External RC what should i do as that RESET doesnt follow my VCC
as can be seen in below mentioned picture
Yellow is my VCC
Green is Reset
It is following VCC which i dont want
As what should i do so that there is delay as well as i can program using 4 wire method.