Tool/software:
Hi Team,
What is the sampling frequency range of the 24-bit Sigma-Delta ADC (SD24_B module) in the MSP430F6779 microcontroller? Up to what harmonic this MCU can calculate with the 24-bit resolution for the ADCs?
Thanks,
Maryam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
What is the sampling frequency range of the 24-bit Sigma-Delta ADC (SD24_B module) in the MSP430F6779 microcontroller? Up to what harmonic this MCU can calculate with the 24-bit resolution for the ADCs?
Thanks,
Maryam
Hi Maryam, this depends on several factors including the fMOD freq. the OSR, and the effective output sample rate. with this in mind,
OSR = 256 --16kHz
OSR = 128 -- 32kHz
OSR = 64 -- 64khz
OSR = 32 -- 128kHz (MAX)
Hope this helps!
Brian,
Thank you. but fMOD freq is not 1MHz? and lower OSR does not reduce precision of ADC?
**Attention** This is a public forum