Part Number: MSP430FR6047
Other Parts Discussed in Thread: EVM430-FR6047,
Tool/software:
Hi there,
I'm comparing the Datasheet for the MSP430FR6047 and the eval board EVM430-FR6047 and I want to make sure this is that this is not a mistake.
Below is from the datasheet from the datasheet of MSP430FR6047 and it shows that the channel 0 out goes into the channel 1 in and the channel 1 out goes into channel 0 in.

but on the EVM430-FR6047 eval board it shows that the channel 0 out goes into the channel 0 in and the channel 1 out goes into channel 1 in, and this goes directly into their respective pins on the MSP chip.

Is this an error? I just want to make sure I understand how I should design my circuit.