Tool/software:
Dear TI Engineers,
I have a question regarding the "Meter Constant" parameter in the Ultrasonic Sensing Design Center.
According to the Application Report: Waveform Capture Based Ultrasonic Sensing Water Flow Metering Technology (SLAA889A), the flow velocity and flow rate are calculated as follows:
Flow velocity:
v = L/2 x (1/T12 - 1/T21)
Flow rate:
Q = S x v = S x L/2 x (1/T12 - 1/T21)
Where:
L is the distance between transducers,
S is the cross-sectional area of the pipe,
T12 and T21 are the ultrasonic propagation times.
Given this, is it correct to assume that the Meter Constant used in the Design Center corresponds to:
Meter Constant = S × L / 2
If not, could you please clarify how the Meter Constant is derived and what physical parameters it represents?
Thank you for your support.