1. I want to interface output of op-amp tlc071 with adc12 of msp430f235. the maximum current at any pin of msp430 could be 2mA. but tlc071 supplies current more than 2mA. In order to prevent microcontroller from damage what should be done?
2. If i do current limitation using a resistor than can it load to that particular input pin's voltage?
3. What is the input impedance of any pin of msp430?