This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: USS water flow Temperature

Part Number: MSP430FR6047

Tool/software:

I am trying to building a water meter sensor using the MSP30FR6047EVM and USS library. And I need to extract the temperature calculation result from USS_Algorithms.
I did the following updated in USS_userConfig.h :

  • Set  USS_ALG_ENABLE_ESTIMATE_TEMPERATURE  to true
  • Set USS_ACOUSTIC_LENGTH  to 70  (as the distance of the transducers is about 70mm)
  • Set USS_VOLUME_SCALE_FACTOR   to  2.5484e7f


As an initial debugging step, I print out all USS_Algorithms_Results over the UART, here are the output
AbsTof_UPS  5.4188e-05
AbsTof_DNS  5.4188e-05
DToF  -2.9502e-11
VOL_FR  -5.1807e+00
TEMP   3.6301e+02

I don’t know why the temperature value is 363 degrees
I checked that there is no error (our message code output is: USS_message_code = 122) for USS_runAlgorithms

**Attention** This is a public forum