Part Number: MSP430FR6047
Other Parts Discussed in Thread: UNIFLASH, MSP-FET
Tool/software:
I'm having trouble connecting UniFlash with MSP-FET to a custom PCBA using the MSP430FR6047. I have confirmed 3.3V and GND connections are correct to the VCC_TARGET and GND pins of the MSP-FET (pins 4 and 9 respectively).
I have connected a 47 kOhm pull-up resistor and 1000 pF capacitor to ground on the RST signal. The RST signal is connected to the pin 11 of the MSP-FET. I have confirmed with a scope that the RST signal switches from 3.3V to ground while UniFlash attempts to connect.
I have also confirmed TEST pin 8 is connected properly to the MSP430FR6047. I also see this signal switching from 0V to 3.3V while UniFlash attempts to connect.
I always get the "Error: connecting to the target: Unknown device".
Any suggestions for next troubleshooting steps?
Thank you.