The application note Sensored 3-Phase BLDC Motor Controller Using MSP430 specifies maximum speed as 41000 rpm for Hurst DMA0102024C 6 pole motor -sec 2.3.2 Page 9, foot note 2. Could you please explain how this value is calculated? Assuming a 8.125 us hall interrupt even processing time I am getting a factor of 10 error.