Part Number: MSP430F5342
I have a Xilinx demoboard that uses the MSP430F5342 as a system controller. On perhaps 1 out of 10 powerups it looks like the MSP is not resetting properly. There is a simple RC + SN74LVC1G08DCKR buffer driving the NMI/RST_B line, using 47.5K and 2.2nF tied to the 3.3V rail. The 3.3V has a risetime of several milliseconds, and powers the MPS, the buffer, and the RC; I'm guessing that the RC timeconstant is too short for milliseconds of risetime.
I'm thinking of bypassing the buffer (since it's not a schmitt trigger) and connecting a slower RC directly to the RST_B pin. Does the MSP have a maximum RC that can be applied to this pin?