This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5659: How to detect USB connection

Part Number: MSP430F5659

Hi experts,

The MSP430F5659 typically operates in low-power mode. My customer wants the MSP430 to exit low-power mode after detecting a USB connection. How can this be achieved?

Thanks,

Leo

  • Hi Leo, you should be able to use an interrupt once the MSP detects the 5V power which triggers the PUR_EN bit. The available interrupts for USB specifically can be found in the reference manual on table 42.2:USB Interrupt Vector Generation. You should then be able to use this as an interrupt to wake the device from LPM. Hope this helps!

    -Brian

**Attention** This is a public forum