Hello,
We are using MSP430F5529 and in our application we have to reprogram the
USB BSL to UART BSL.
The UART BSL could be programmed using the CCS or the FlashPro430(Elprotronic).
But the problem is the MSP-GANG, we cannot program the BSL memory with MSP-GANG Programmer.
Below is the error window from the older Gang430, which also same for MSP-GANG.
We always get the memory verification error.
Even tried with the Lite FET-Pro430+MSP-FET430UIF, we get the same error.

It works fine with FlashPro430 + the adapter from Elpro.
Is this a limitation of MSP-GANG/Gang430?
As we are into mass production we cannot use FlashPro430, we need to use GANG.
Please let me know if there is any way out.
Regards.