Part Number: MSP430FR5887
The ESI module is supposed to operate in a -20 degrees Celsius environment, but the test failed and the counting stopped. How can we improve this?
Additionally, if the calibration is performed using AFE2, it is impossible to perform the calibration when the metal pointer remains stationary, right? Then, the pointer starts to move only when the temperature difference is 30 degrees Celsius. Delta = (ESIDAC1R0 + ESIDAC1R1) / 2 - New_level; Will Delta < 10 cause the re-calibration to fail?