This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430AFE221: Suitable micro controller for the application

Part Number: MSP430AFE221

Hi Team,

We need a low cost microcontroller for our R&D application. The annual quantity of this product is 50K. The microcontroller should have the below inputs.

  1. It will be suitable to our battery based application( low Q current and sleep current)
  2. It should have 5 ADC channels-12/16bit ADCs are sufficient
  3. Total number of pins will be <64
  4. >16bit microcontroller
  5. Inbuilt wireless module is highly suitable(not a mandatory)
  6. All the interfaces like I2C, SPI and USB interfaces should be there
  7. Memory should be higher in the range

Kindly recommend us the right microcontroller.

 

Regards,

murugavel.S

**Attention** This is a public forum