Part Number: DRV8363-Q1EVM
Other Parts Discussed in Thread: MSPM0G3519, , LAUNCHXL-F280049C, DRV8363-Q1, DRV8363
Hi,
I am working on a BLDC motor control application using the MSPM0G3519 MCU and have procured the DRV8363-Q1EVM for gate-driver evaluation.
While going through the DRV8363-Q1EVM Quick Start Guide, I noticed the following caution note:

Currently, I do not have the LAUNCHXL-F280049C board, and I intend to interface the DRV8363-Q1EVM directly with the MSPM0G3519 MCU.
I would like clarity on the following points:
-
Is the DRV8363-Q1EVM electrically and functionally compatible with MSPM0G3519 for evaluation purposes (SPI + 6-PWM control)?
-
Does the caution note indicate a hardware limitation, or is it primarily related to official software support and validation from TI?
-
Are there any specific constraints, risks, or recommended checks when using DRV8363-Q1EVM with a non-C2000 MCU such as MSPM0?
-
Is there any reference documentation, application note, or recommended validation procedure for bringing up DRV8363-Q1EVM with general-purpose MCUs?
-
For basic BLDC operation (6-step commutation), is software-based dead-time generation from MSPM0 considered acceptable for evaluation?
My goal is to safely validate the DRV8363-Q1 device and perform low-power BLDC motor control experiments using MSPM0G3519.
I would appreciate your guidance on whether this approach is acceptable and any recommendations you may have.
Thank you for your support.
Best regards,
Sakhan